Discover xStorage Home

Nissan's battery technology at the service of the smartest and most powerful energy storage solution

Place your pre-order now

A sustainable future with Nissan

At Nissan, the future is electric. Join Nissan in building a more sustainable future, together.

Learn More

Designed to be the most reliable and affordable


xStorage Home has been designed to be the most reliable and affordable home energy storage system.

xStorage Home is a complete system, housed in a single unit, that integrates everything needed to manage and store energy in your home.


Lower your electricity bills
When connected to your residential power supply and/or renewable energy sources such as solar panels, the unit can help you save money on electricity bills. It does this by charging up when renewable energy is available or energy is cheaper (i.e. during the night) and releasing that stored energy when demand and costs are high.

Lower your CO2 footprint
By storing, consuming or even selling renewable energy back to the grid, you can contribute to the decarbonisation of the energy supply.

Make a positive contribution to the environment: use second-life Nissan Leaf batteries
xStorage Home provides a sustainable second life for Nissan’s electric vehicle batteries after their first life in cars is over.

No more lights out
In the event of a power shortage or outage, the unit acts as a back-up power source. Ideal at a time when our energy grids are coming under enormous and increasing strain.

Easy to install and use
Once set-up by a certified installer, the unit is ready to go and can be plugged in and powered up simply and easily. It also has smartphone connectivity for usability and to allow you to switch between energy sources at the simple touch of a button..

Safe technology
xStorage Home technology is rigourously tested to deliver high levels of safety, reliability and performance. As a power management company with over 100 years experience and as a leader in Uninterruptible Power Supply technology, Eaton brings a depth of experience to energy storage that is unmatched. Nissan is the leader in Electric Vehicles and is a proven, high volume, maker of reliable Li-Ion batteries that meet the strict safety standards of the automotive market. By pooling our expertise and technologies, we promise our customers a superior system that has been rigorously researched, tested and approved.

Customer service
The system is supported by a network of over 1,000 distributors, working with qualified installers.

Make energy storage simple for you and pre-order now the xStorage Home and receive it this year

Start at €4,943 excluding installation costs and VAT. Reserve yours now with a €50 registration fee.



Pre-order now


Want more information? Tell us how we can help you and one of our experts will call you back.

Contact Us


Learn more about Nissan Energy Solutions.

Visit Nissan's Website

Let’s get more technical.

xStorage Home is designed to be the most reliable and affordable energy storage solution on the market today. xStorage Home combines second-life Nissan Leaf battery modules with Eaton power quality technology and electronics. It’s simple to install and use.

How it works

When connected to your residential power supply and/or renewable energy sources such as solar panels, the unit helps save money on electricity bills. It does this by charging up when renewable energy is available or energy is cheaper (i.e. during the night) and releasing that stored energy when demand and costs are high.

If your home is equipped with solar technology you can power it using clean energy stored in your xStorage Home system. The financial rewards are obvious, as it helps you avoid expensive daytime energy tariffs.

xStorage Home also acts as a back-up source - ensuring that the lights never go out. This is a huge advantage at a time when the energy grid is coming under enormous strain.

In some countries you can also generate additional revenues by selling stored energy back to the grid when demand and costs are high.

Specifications

Cell technology Lithium-ion
Battery type Second life New
Storage Capacity 4.2 kWh 6 kWh
Battery life 5 years
1 full cycle
(charge and discharge) per day
10 years
1 full cycle
(charge and discharge) per day
Power distribution Single phase
Maximum recommended PV Power 4.8 kW PV
Input AC, 184Vac-264,5Vac
DC for PV, 150 – 500 Vdc
AC output power 3-3, 6-4, 6kW
Operating Temperature -10 °C - 30°C
System efficiency 97%
System weight Inverter 45kg Battery Pack 75kg
Installation type Wall mounted
Installation environment Indoor
Certifications 2011/65/EU (RoHS)
EMC Directive 2014/30/EU
Security Guide 2014 – Li-Ion domestic storage harmonised standards
and valid transport and packaging regulations


Maximum power for single phase systems partly dependent on national specifications.

Download the Eaton Nissan xStorage Home brochure

News room

You can access press releases, articles and a media kit about xStorage Home here.
We will be happy to help you with any media inquiries.

Articles

May 15
Cleantechnica.com
Nissan Reuses EV Batteries For Home Energy Storage — xStorage

May 12
Renewablenergyworld.com
Nissan, Eaton to Release Residential Energy Storage Product ‘xStorage’

May 11
Governmentenergy.net
Nissan and Eaton launch home energy storage unit

Smartcitiesworld.net
Nissan joins Eaton to launch new residential energy storage unit

Techradar.com
Nissan's home battery will drive down your electricity bill

Businessgreen.com
Nissan launches domestic energy storage system in vehicle-to-grid push

May 10
Mashable.com
Nissan unveils a home battery to take on Tesla's Powerwall

Stuff.tv
Nissan's xStorage batteries can power your house - and earn you cash

Blueandgreentomorrow.com
Earn from Excess Energy with Nissan

Press releases

Nissan and Eaton broaden xStorage residential energy storage portfolio as pre-orders commence in Europe

• xStorage Home portfolio now includes a range of six product configurations with prices starting from €3,500 (excl. VAT and installation costs)
• Pre-orders begin in UK, Norway and Germany today
• Helps consumers control how and when to use energy in their homes to avoid expensive energy tariff periods
• Uses Nissan’s safe and proven battery technology powering more than 260,000 electric vehicles all over the world

Barcelona (Nov. 30th, 2016) Nissan and power management leader Eaton are broadening their portfolio of xStorage Home residential energy storage solutions by introducing a range of six product configurations, giving consumers greater choice to meet their energy needs. This announcement comes as pre-orders of xStorage Home begin today in UK, Norway and Germany with other European markets to follow in the coming months.

The xStorage Home system can draw energy from the sun or from the grid, making energy consumption more affordable and encouraging home-owners to make a more sustainable choice. The cutting-edge technology in the xStorage Home system is also fit for the future, and can enable customers to sell energy back to the grid – an opportunity that is expected to be offered by energy companies in the future.

The system gives consumers greater control over how and when they use energy in their own homes enabling them to avoid expensive tariff periods. The expanded range will offer consumers greater choice over power capacity and price as well as units. Consumers can opt to purchase units powered by either second life batteries or new batteries.

xStorage Home units – which provide a sustainable second life for Nissan’s electric vehicle (EV) batteries after their first life in cars is over – will be priced competitively starting at €3,500 (excluding VAT and installation costs) for a power capacity of 3.5kW rising to just €3,900 for 6kW. Units powered by new Nissan batteries will start from €5,000 rising to €5,580 for the highest capacity and will come with an extended warranty period of ten years.

Connected to a residential power supply and/or renewable energy sources such as solar panels, the unit has the potential to revolutionise the way people manage energy usage in their own home, providing added flexibility.

xStorage Home comes with solar panel inverters already integrated meaning that if a home is equipped with solar panels, the consumer can connect directly to xStorage Home, storing and then powering their homes using clean, renewable energy. It can also save customers money on their utility bills by charging up when renewable energy is available or cheaper, and releasing that stored energy when demand and costs are high.

The xStorage Home unit also has the capability to provide energy back to the grid in countries where the conditions enable customers to do so. This provides another potential revenue stream as customers will be able to sell stored energy back to the grid when demand and costs are high.

The system also provides the ultimate back-up energy solution to consumers, ideal at a time when energy grids are coming under significant strain. With smartphone connectivity, it allows consumers to switch between energy sources at the touch of a button.

Paul Willcox, Chairman, Nissan Europe said: “Energy pricing and availability have long been concerns for all of us, and with this product, consumers will finally be able to take control of how and when they use energy in their homes.
We have already seen overwhelming interest for this product, so we’re excited to be able to offer consumers even greater choice with our wider portfolio of xStorage products. With the launch of xStorage Home, we’re fast approaching a consumer energy revolution.
xStorage Home will deliver real world benefits for smarter, more affordable and more sustainable energy management.”

This move towards the use of alternative energy sources is in line with consumer demand across Europe. Nissan’s Social Index report found that environmental issues are one of European consumers’ greatest concerns for the future. An overwhelming majority of those surveyed (91 percent) were excited to see more alternative energy sources developed in the future and three 89 percent wanted to see recycled materials used in more innovative ways.

Frank Campbell, President, Eaton Electrical and Corporate EMEA said: “European consumers are increasingly demanding alternative energy management solutions. Working in partnership with Nissan, we have developed a range of affordable, ready to use home energy storage solutions, giving consumers a choice of six options. While other home energy storage products are available on the market, we aim to avoid hidden extra costs and achieve the lowest possible total cost of ownership.”

The new xStorage Home portfolio marks the start of a longer-term commitment by Nissan and Eaton to bring new products to market for both private and commercial customers. Nissan’s commercial offering, xStorage Buildings, is a robust and powerful solution for organisations to manage their energy usage more efficiently and power their business in a more sustainable, smarter way.

Today, Nissan and Eaton announced a major partnership with Amsterdam ArenA - home of Ajax Football Club - which will see the integration of xStorage Buildings into the stadium. Representing the largest energy storage system in a commercial application in Europe using second life electric vehicle batteries, the xStorage Buildings system comprises Eaton bidirectional inverters and the equivalent of 280 Nissan LEAF second life battery packs. It will make the energy supply to Amsterdam ArenA more efficient, sustainable and reliable through additional back-up power replacing diesel generators and grid stabilization services.

To find out more about Nissan’s and Eaton’s energy storage product portfolio, please visit: www.eaton.eu/energystorage.

About Nissan in Europe

Nissan has one of the most comprehensive European presences of any overseas manufacturer, employing more than 17,600 staff across locally-based design, research & development, manufacturing, logistics and sales & marketing operations. In 2014 Nissan plants in the UK, Spain and Russia produced more than 675,000 vehicles including award-winning crossovers, small cars, SUVs, commercial vehicles and electric vehicles, including the Nissan LEAF, the world's most popular electric vehicle with 96% of customers willing to recommend the car to friends. Nissan now offers a strong line-up of 23 diverse and innovative models in Europe under the Nissan and Datsun brands

About Nissan Motor Co., Ltd.

Nissan is a global full-line vehicle manufacturer that sells more than 60 models under the Nissan, Infiniti and Datsun brands. In fiscal year 2014, the company sold more than 5.3 million vehicles globally, generating revenue of 11.3 trillion yen. Nissan engineers, manufactures and markets the world's best-selling all-electric vehicle in history, the Nissan LEAF. Nissan’s global headquarters in Yokohama, Japan manages operations in six regions: ASEAN & Oceana; Africa, Middle East & India; China; Europe; Latin America and North America. Nissan has a global workforce of 247,500, and has been partnered with French manufacturer Renault under the Renault-Nissan Alliance since March 1999

About Eaton

Eaton is a power management company with 2015 sales of $20.9 billion. Eaton provides energy-efficient solutions that help our customers effectively manage electrical, hydraulic and mechanical power more efficiently, safely and sustainably. Eaton has approximately 97,000 employees and sells products to customers in more than 175 countries. For more information, visit www.eaton.com.

Media kit


Contact us

Julia Tisserant, Eaton EMEA
+41 21 811 4639
JuliaTisserant@Eaton.com

Vera Grishchenko, Eaton EMEA
+44 7583 090560
VeraGrishchenko@Eaton.com

Cedric Ratinaud, Nissan Europe
+33 616 643 481
CRatinaud@nissan-europe.co.uk

Katherine Zachary, Nissan Europe
+33 172 672 922
KZachary@nissan-europe.com

Pre-order now

Make energy storage simple for you and pre-order now the xStorage Home and receive it this year.

Start at €4,943 excluding installation costs and VAT


Pre-order now

Contact us and see how you can benefit from our energy storage systems.

Contact us